Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
KlausK_81
Employee
Employee
25 sign-ins 10 questions asked 10 sign-ins

CYBLE-212019-SHIELD EZ-Serial™ Arduino Shield

refer to Arduino Library EZSLib which should be located at

EZ-SERIAL™: EZ-BLE MODULE FIRMWARE PLATFORM

Container file EZ-Serial Host API Protocol Library

don't include the library file .

Where could I download the missing folder arduino\EZSLib for the Arduino support ?

Thanks

Klaus

0 Likes
6 Replies
Anonymous
Not applicable

The link https://community.cypress.com/external-link.jspa?url=http%3A%2F%2Fwww.cypress.com%2Ffile%2F384511%2F... has the zip file with the python api file and psoc creator api files included. jrow

0 Likes

The folder arduino\EZSLib for the Arduino support don't exist in the zipped library file .

0 Likes
Anonymous
Not applicable

The entire folder of the zip file contains the files for the EZSLib;

Just rename the extracted folder name to "EZSLib" from "EZ-Serial_Host_API_Protocol_Library" and then follow the steps in the guide.

The .c, .h, .json, .py files are all in there. (You can remove the cy8ckit-042-psoc4 folder within it if necessary I think)

0 Likes

Folder renamed and copied to Arduino Library link.

Step6; Use the File -> Examples -> EZSLib -> Examples -> EZSLib_generic_demo menu item to open a simple example sketch.

I can't select the example sketch , it seems there is no required files in our EZSLib .

My setup:

Arduino 1.8.5

Board: Freesoc2 ( PSOC5LP )

Thanks

Klaus

0 Likes
Anonymous
Not applicable

Hmmmm; Weird. It seems like the files for EZSLib were pulled out of the example/zip.

Possibly hima​ has information on getting an arduino example working?

Otherwise, you can try making a support case to see if they can get it resolved.

0 Likes

Could you estimate when all material is updated on the webpage to enable

a error free usage ?

Best Regards,

Klaus

0 Likes