Cy8ckit-044 5 Volt tolerant

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Dear forum users

   

 Can some one tell me if the CY8CKIT-044 io pins are 5V tolerant ?

   

Whit best regards Ben

0 Likes
3 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

All Cypress PSoCs GPIO pins can tolerate 0V to Vdd. So when powered with 5V the GPIOs will run up to this voltage.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

So if i place JP9 in to the 5 volt position the pins can tolerate up to 5 V is that right ?

   

Whit best regards Ben

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Yes, that's right.

   

 

   

Bob

0 Likes