cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

Anonymous
Not applicable

Hello, I am working with CY8CKIT-042-BLE, it´s the BLE Pioneer Kit. 

   

The problem, I have, is to create a Central GAP role, using the USB dongle 56LQXI , I did already a Server GAP Role project  and it works when I used CySmart.

   

I read some tutorials about how to initialize the StackEventHandler but when I developed the code

   

the connection between the USB dongle and the PRoC BLE Module is not possible, according to my code. However, using the Cysmart the connection is posible.

   

Also I´m having problem how to write on my server, I´m using the function  CYBLE_GATTC_WRITE_REQ_T 

   

but I dont know how get the attrHandle

   

I´ve attached the file with the Peripheral and Central  projects.

   

 

   

Thanks you for your help

   

David Caraveo

0 Likes
2 Replies
himam_31
Employee

Hello,

   

Can you please tell us what exactly the problem is? Are you facing issues with connection or only while data is being transferred.

   

Thanks,

   

Hima

0 Likes
Anonymous
Not applicable

I´m having issue with the connection part. I cannot stablish the connection between them,

0 Likes