cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

OsFe_2822791
New Contributor II

Hi,

Is it possible to use 5 opamps simultaneously in CY8CKIT-044?

Thank you.

Regards.

0 Likes
1 Solution
MotooTanaka
Esteemed Contributor

Hi,

According to the datasheet of PSoC 4 PSoC 4200M,

it has only 4 opamps.

You can download the datasheet from the URL below.

https://www.cypress.com/part/cy8c4247azi-m485

So I think that maximum opamps which can be used with CY8CKIT-044 is 4.

moto

View solution in original post

0 Likes
2 Replies
MotooTanaka
Esteemed Contributor

Hi,

According to the datasheet of PSoC 4 PSoC 4200M,

it has only 4 opamps.

You can download the datasheet from the URL below.

https://www.cypress.com/part/cy8c4247azi-m485

So I think that maximum opamps which can be used with CY8CKIT-044 is 4.

moto

View solution in original post

0 Likes
odissey1
Honored Contributor II

OsFe,

You can refer to the KIT-044 annotation component, which shows PSoC4 pinout and Opamps.

KIT-044: annotation component for CY8CKIT-044 PSoC4M Pioneer Kit

/odissey1

KIT-044_AllOptions_A.png