CYBLE-022001 connected as central and peripheral mode at the same time

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello,

   

 

   

I noted that CYBLE chip can act as central and peripheral mode in the same chip.  In the example (Day012_Central_Peripheral), , it is connected as either central and peripheral mode (master or slave).  But can this chip be connected as both central and peripheral mode at the same time?  I would to make the chip acting as a BLE repeater to extend the signal distance.

   

 

   

Best regards.

   

Tim

0 Likes
1 Solution
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

I don't think thats possible, the BLE stack can handle only one connection at a time.

View solution in original post

0 Likes
3 Replies
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

I don't think thats possible, the BLE stack can handle only one connection at a time.

0 Likes
Anonymous
Not applicable

Hmm.... I ask this question because I know Nordic S130 BLE stack can do it.  So, I thought Cypress BLE stack can do as well.  A little bit disappointed.

   

Thanks anyway.

0 Likes