cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

AmMa_2724956
New Contributor II

Hello,

I am using CYBLE-012011-00 modules which sends and receives some values over BLE from App.

So while testing with some devices (testing on CySmart app), on some devices it gets disconnected abruptly/services are not discoverable.

On some devices it works fine and does not get disconnected and services are also discovered.

While debugging it was found that on devices on which it disconnects abruptly and unhandled event is called : CYBLE_EVT_GAP_CONNECTION_UPDATE_COMPLETE

And the disconnection error is : CYBLE_HCI_INSTANT_PASSED_ERROR

On devices it works fine, the above two events/error are not generated.

Thanks,

Ameya

0 Likes
1 Solution
2 Replies
AmMa_2724956
New Contributor II

PFA images of the log of CySmart App and the UART showing unhandled events and error code in case of disconnection.CySmart Disconnect Log.jpgBLE Disconnect Sequence.jpg

0 Likes
GyanC_36
Employee

Hi Ameya,

     Please refer the below thread and let me know if it helps.

Re: instant passed error

-Gyan