cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

hesc_1314511
New Contributor II

I made a circuit where a CY8C4125AZI-S413 directly drives an iconographic LCD. The display has normal LCD segments. I tried to make it work and after 15 minutes the CY8C4125AZI-S413 got damaged, it became a short circuit. Is it a problem if CY8C4125AZI-S413 directly drives an LCD dislay with 3.3V?

0 Likes
3 Replies
DheerajK_81
Moderator
Moderator

CY8C4125AZI-S413 has the capability to drive an LCD. I don't necessarily think LCD is causing this issue. Can you please send your schematic for review?

Regards,

Dheeraj

0 Likes
hesc_1314511
New Contributor II

hello,

I attach the scheme of the display

regards

Henry

Il 01/03/2019 08:09, DheerajK_81 ha scritto:

<http://www.cypress.com>

Cypress Developer Community <https://community.cypress.com/?et=watches.email.thread>

CY8C4125AZI-S413 interface with LCD display

reply from DheerajK_81<https://community.cypress.com/people/DheerajK_81?et=watches.email.thread> in PSoC 4 MCU Community - View the full discussion<https://community.cypress.com/message/188813?et=watches.email.thread#188813>

0 Likes
DheerajK_81
Moderator
Moderator

Hello Henry,

I reviewed your schematic. Its not clear what the voltage V12 is and how much voltage arrives at the output (VDD) of the buck regulator (U1). Make sure VDD is between the range 1.8V to 5.5V. Please check this voltage.

Regards,

Dheeraj

0 Likes