Today I discovered a bug in PSoC Creator 4.2 when using the home folder and using a certain path length in Windows to build your code.
This took a day of my life to figure out what was wrong. I checked the code, project files, compiler and linker settings, like a million times, but that was not the case. It was just the home folder in combination with path length.
It does not happen in other locations other than your home folder.
When does it happen:
Example path in my case (reproducible error):
My project folder (not that very deep to be honest)
c:\Users\paul\Projects\Cypress\BLE-Projects\
When you unpack the 100 days examples in it.... (Still not that much: 127 characters, still far below ~247 of Windows)
c:\Users\paul\Projects\Cypress\BLE-Projects\PSoC-4-BLE-master\100_Projects_in_100_Days\Day020_BLE_UART\UART_to_BLE_peripheral\
Then when you build your project it will end up with a compile error.
So you keep thinking what have I done wrong. The compiler doesn't complain about path sizes or disk storage issues.
And the error doesn't reveal that much "failed with exit code '1'.
BUT here is the catch, when you put the entire folder in another location than C:\users\{yourname} suddenly it the compile error is gone! Yai!
Even when the path length is even longer than before.
My conclusion is that there is an issue with the relative path's that are a bit long when building the code. If it are full path's the issue doesn't appear.
arm-none-eabi-gcc.exe -Wl,--start-group -o C:\Users\paul\Projects\Cypress\BLE-Projects\PSoC-4-BLE-master\100_Projects_in_100_Days\Day020_BLE_UART\UART_to_BLE_peripheral\UART_to_BLE_peripheral.cydsn\CortexM0\ARM_GCC_541\Debug\UART_to_BLE_peripheral.elf .\CortexM0\ARM_GCC_541\Debug\main.o .\CortexM0\ARM_GCC_541\Debug\app_Ble.o .\CortexM0\ARM_GCC_541\Debug\app_UART.o .\CortexM0\ARM_GCC_541\Debug\app_LED.o .\CortexM0\ARM_GCC_541\Debug\cyfitter_cfg.o .\CortexM0\ARM_GCC_541\Debug\cymetadata.o .\CortexM0\ARM_GCC_541\Debug\Cm0Start.o .\CortexM0\ARM_GCC_541\Debug\UART_to_BLE_peripheral.a "..\..\..\..\..\..\..\..\Documents\PSoC Creator\4.2\Downloads ( 4.2).cylib\BLE_v3_20\Library\gccCyBLEStack_BLE_SOC_PERIPHERAL.a" -mcpu=cortex-m0 -mthumb -L Generated_Source\PSoC4 -Wl,-Map,.\CortexM0\ARM_GCC_541\Debug/UART_to_BLE_peripheral.map -T Generated_Source\PSoC4\cm0gcc.ld -specs=nano.specs -Wl,--gc-sections -g -ffunction-sections -O0 -ffat-lto-objects -Wl,--end-group
Below the full path:
"c:\Program Files (x86)\Cypress\PSoC Creator\4.2\PSoC Creator\import\gnu\arm\5.4.1\bin\arm-none-eabi-gcc.exe" -Wl,--start-group -o C:\Users\paul\Projects\Cypress\BLE-Projects\PSoC-4-BLE-master\100_Projects_in_100_Days\Day020_BLE_UART\UART_to_BLE_peripheral\UART_to_BLE_peripheral.cydsn\CortexM0\ARM_GCC_541\Debug\UART_to_BLE_peripheral.elf .\CortexM0\ARM_GCC_541\Debug\main.o .\CortexM0\ARM_GCC_541\Debug\app_Ble.o .\CortexM0\ARM_GCC_541\Debug\app_UART.o .\CortexM0\ARM_GCC_541\Debug\app_LED.o .\CortexM0\ARM_GCC_541\Debug\cyfitter_cfg.o .\CortexM0\ARM_GCC_541\Debug\cymetadata.o .\CortexM0\ARM_GCC_541\Debug\Cm0Start.o .\CortexM0\ARM_GCC_541\Debug\UART_to_BLE_peripheral.a "c:\users\paul\Documents\PSoC Creator\4.2\Downloads ( 4.2).cylib\BLE_v3_20\Library\gccCyBLEStack_BLE_SOC_PERIPHERAL.a" -mcpu=cortex-m0 -mthumb -L Generated_Source\PSoC4 -Wl,-Map,.\CortexM0\ARM_GCC_541\Debug/UART_to_BLE_peripheral.map -T Generated_Source\PSoC4\cm0gcc.ld -specs=nano.specs -Wl,--gc-sections -g -ffunction-sections -O0 -ffat-lto-objects -Wl,--end-group
I've executed the above statement from the command-line from the exact path in the project and it compiles without issues. I've modified the relative path to be the full path though.
See attached the log files.
Cheers,
Paul
Hello Paul,
I created project at this path as you have instructed:
C:\Users\anks\Projects\Cypress\BLE-Projects\PSoC-4-BLE-master\100_Projects_in_100_Days\Day020_BLE_UART
As you can see the same in this screenshot:
Then I given a build to the project in PSoC Creator 4.2 (4.2.0.641) after Updating the components. I was able to build the project as shown in this image below:
Am I missing any steps? I am unable to reproduce the issue on Windows7 System
As far as I remember there is a limit in win7 for the length of a pathname. And I am quite sure that this could be tuned using a setting in the registry. Too long ago and brain is worn... Think might invetigate in that direction.
Bob
Thanks, bob, I've checked that. The path's stay far below the 247 characters (considering drive and extensions).
If I place it outside the home folder I can use even longer paths and it will build without errors.
But even when the path is too long, I expect that an IDE like PSoC Creator will warn me about this instead of giving me an unclear error message.
Hi Anks,
Thanks for looking into this and trying to reproduce.
1.)
Can you check if your " PSoC Creator" folder is located in \Documents\ :
c:\Users\anks\Documents\PSoC Creator\4.2\Downloads ( 4.2).cylib\ ... --> contains subfolders
Having both 1) above folder and 2) project folder in the user folder will generate a generic path instead of a full path for arm-none-eabi-gcc.exe for the linking proces.
2.)
Can you make a copy of the entire line, so we can compare ? The line looks like this:
arm-none-eabi-gcc.exe -Wl,--start-group -o C:\Users\ ..... (it's quite a long line)
Or just copy and paste the entire output window and put it in a txt file as an attachement.
ps. I'm using Windows 10 pro. Version: 1803, OS Build: 17134.48
Thanks,
Paul
Yes Paul, this path has PSoC Creator folder and subfolders within it in my system:
c:\Users\anks\Documents\PSoC Creator\4.2\Downloads ( 4.2).cylib\ .
I am attaching the build log.
Checking the log provided by you with error , it seems the issue is this as stated "gccCyBLEStack_BLE_SOC_PERIPHERAL.a: No such file or directory"
So, firstly check whether this file gccCyBLEStack_BLE_SOC_PERIPHERAL.a file is present at this path in your system or not
C:\Users\anks\Documents\PSoC Creator\4.2\Downloads ( 4.2).cylib\BLE_v3_XX\BLE_v3_xx\Library
If the .a file is present at this path,still creator is unable to access then it may be a Permission Access issue.
Otherwise,I believe to fix this issue you need to recreate the library project.
#1 delete folder "Downloads ( 4.2).cylib"
#2 Open PSoC Creator 4.2
#3 Tools -> Find new components
#4 Search 'BlueTooth'
#5 Select version BLE component's latest version available(v3_50)
#6 Click 'Install Checked Components'
Now you should see the Downloads ( 4.2).cylib being recreated.
Yess I've got the file (gccCyBLEStack_BLE_SOC_PERIPHERAL.a) and I have all the latest components.
"c:\Users\paul\Documents\PSoC Creator\4.2\Downloads ( 4.2).cylib\BLE_v3_51\Library\gccCyBLEStack_BLE_SOC_PERIPHERAL.a"
And I have another one here:
"c:\Program Files (x86)\Cypress\PSoC Creator\4.2\PSoC Creator\psoc\content\CyComponentLibrary\CyComponentLibrary.cylib\BLE_v3_50\Library\gccCyBLEStack_BLE_SOC_PERIPHERAL.a"
-It is also not a permissions issue. If I shorten the path of the project file it will compile.-
For some reason your generated build script differs from mine.
And then specifically this line:
Yours:
arm-none-eabi-gcc.exe -Wl,--start-group -o C:\Users\anks\Projects\Cypress\BLE-Projects\PSoC-4-BLE-master\100_Projects_in_100_Days\Day020_BLE_UART\UART_to_BLE_peripheral\UART_to_BLE_peripheral_01.cydsn\CortexM0\ARM_GCC_541\Debug\UART_to_BLE_peripheral_01.elf .\CortexM0\ARM_GCC_541\Debug\main.o .\CortexM0\ARM_GCC_541\Debug\app_Ble.o .\CortexM0\ARM_GCC_541\Debug\app_UART.o .\CortexM0\ARM_GCC_541\Debug\app_LED.o .\CortexM0\ARM_GCC_541\Debug\cyfitter_cfg.o .\CortexM0\ARM_GCC_541\Debug\cymetadata.o .\CortexM0\ARM_GCC_541\Debug\Cm0Start.o .\CortexM0\ARM_GCC_541\Debug\UART_to_BLE_peripheral_01.a "C:\Program Files (x86)\Cypress\PSoC Creator\4.2\PSoC Creator\psoc\content\CyComponentLibrary\CyComponentLibrary.cylib\BLE_v3_50\Library\gccCyBLEStack_BLE_SOC_PERIPHERAL.a" -mcpu=cortex-m0 -mthumb -L Generated_Source\PSoC4 -Wl,-Map,.\CortexM0\ARM_GCC_541\Debug/UART_to_BLE_peripheral_01.map -T Generated_Source\PSoC4\cm0gcc.ld -specs=nano.specs -Wl,--gc-sections -g -ffunction-sections -O0 -ffat-lto-objects -Wl,--end-group
Mine:
(For some unclear reason my PSoC Creator applies a relative path).
arm-none-eabi-gcc.exe -Wl,--start-group -o C:\Users\paul\Projects\Cypress\BLE-Projects\PSoC-4-BLE-master\100_Projects_in_100_Days\Day020_BLE_UART\UART_to_BLE_peripheral\UART_to_BLE_peripheral.cydsn\CortexM0\ARM_GCC_541\Debug\UART_to_BLE_peripheral.elf .\CortexM0\ARM_GCC_541\Debug\main.o .\CortexM0\ARM_GCC_541\Debug\app_Ble.o .\CortexM0\ARM_GCC_541\Debug\app_UART.o .\CortexM0\ARM_GCC_541\Debug\app_LED.o .\CortexM0\ARM_GCC_541\Debug\cyfitter_cfg.o .\CortexM0\ARM_GCC_541\Debug\cymetadata.o .\CortexM0\ARM_GCC_541\Debug\Cm0Start.o .\CortexM0\ARM_GCC_541\Debug\UART_to_BLE_peripheral.a "..\..\..\..\..\..\..\..\Documents\PSoC Creator\4.2\Downloads ( 4.2).cylib\BLE_v3_51\Library\gccCyBLEStack_BLE_SOC_PERIPHERAL.a" -mcpu=cortex-m0 -mthumb -L Generated_Source\PSoC4 -Wl,-Map,.\CortexM0\ARM_GCC_541\Debug/UART_to_BLE_peripheral.map -T Generated_Source\PSoC4\cm0gcc.ld -specs=nano.specs -Wl,--gc-sections -g -ffunction-sections -O0 -ffat-lto-objects -Wl,--end-group
It is still a mystery to me why this all happens.
Can you install the Creator4.2 again at default location
Thank you Paul. This was driving me crazy.
Just moving the project to a different directory worked perfectly. No need to reinstall or change the build settings.
--zim