- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I am using the MTK tool in the following community and confirm.
Re: HCI commands to measure packet error rates and RSSI
It is possible to execute slide50 [CYBLE MTK Quick Demo Instructions] under the configuration of [MTK option 1 – UART based testing].
I also want to check [MTK Option 2-BLE link based testing] as well.
However, when I try slide14 [MTK Configuration-BLE link based testing], I get a build error in PSoC Creator.
Please tell me how to deal with it.
[environment]
PSoC Creator version: 4.2
Target Device: CY8C4247LQI-BL483 (CY8CKIT-142)
MTK HOST: CY8CKIT-042-BLE
MTK DUT : CY8CKIT-042-BLE
We changed the PRoC type name to the PSoC 4 BLE type name, and are also performing Component Update.
Best regards,
Kenji Takahashi
Solved! Go to Solution.
- Labels:
-
BLE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Please set the L2CAP MTU size set in the BLE component to 100 or above as shown in the image and check once.
Thanks
Ganesh
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
Hi Ganesh,
Build error has been improved.
However, the LED on the MTK host board does not light up like [MTK Host LED indications] on slide 14.
Also, the first test in MTK tool will fail.
It seems that the DUT can not be found.
It is as follows in CyBLE_MTK.h of MTK project.
#define CYBLE_TESTS_ENABLED 0
Should this be set to 1?
I changed it to 1 and tried build, but an error occurs in Build.
Best regards,
Kenji Takahashi
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
Hi Ganesh,
Thank you for your reply.
By changing the L2CAP MTU Size, I was able to test with MTK Tool.
Best regards,
Kenji Takahashi