- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello colleagues,
I am trying to measure AC current with your PRoC (Eval Kit) and the Allegro's ACS712 but I can just measure noise. I am using the ADC SAR Block with 4.8Vdc as reference and very fast sampling (125ksamples per second). The ADC SAR block screenshots are attached and below is the code:
CY_ISR(ADC_SAR_SEQ_ISR)
{
if (count == 0)
{
min=4096;
max=0;
}
readValue = ADC_SAR_SEQ_GetResult16(0); // Channel 0 is connected my pin to the ACS712 output
if (readValue > max)
max = readValue;
if (readValue < min)
min = readValue;
count++;
if (count >= 25000) // 0.2 seconds
{
mamp = 2.5*(max-min); // (1000*0.353*4800)/(4095*166)=2.5 // 1000 is A to mA, 0.353 is from Vpp to Vrms, 4800mV is Vref, 4095 are the bits of resolution and 166 is the mV/A given by my ACS712
count=0;
}
}
The root problem is that Max and min values are always almost the same (0x5D and 0x5B), no matter which load (no load, 30mA, 200mA or 350mA) is connected. I think the ADC SAR is not really sampling so fast and that's why I measuring always the same, does any of you have an idea of what can be happening?
Thanks in advance,
Peter
- Labels:
-
BLE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I am afraid that 250 thousand interrupts per second are a bit too much to handle for a PRoC. Try polling for the result. Next time can you please post your complete project, so that we all can have a look at all of your settings. To do so, use
Creator->File->Create Workspace Bundle (minimal)
and attach the resulting file.
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
what do you mean by trying polling the result?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
There is an API ADC_IsEndConversion() which queries or waits for conversion ready. This will remove the overhead for handling the interrupts.
Bob
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
You might use DMA to speed things up, but your selected chip might not be equipped with. Can you please post your complete project, so that we all can have a look at all of your settings. To do so, use
Creator->File->Create Workspace Bundle (minimal)
and attach the resulting file.
Bob
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
Please find attached the source code. Some descriptions:
- Pin_Triac is to activate a Triac so the AC can get to the load.
- When no load connected, I can measure max=2048 and min=2047 which is expected (Half of the dynamic range, in this case 12 bits -> 4096)
- When connecting an AC load (i.e 250mA), the first min and max measurements are different from the 2047 and 2038 values, which results to mamp values of 80, 130, 170mA but this changes randomly and it is only the first value. The second, third and so on values are again 2047 and 2048 so something must be wrong with the sampling.
Do you have any idea of what can be happening?
Thanks in advance,
Peter
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
peter,
attached is working project. I tested it using KIT-044M (PSoC4200M), so you might need to re-assign pins to match P4100-BLE. You can play with ADC settings, currently input range is set to 1.024+/-1.024V (Vref=1.024 is the only real buffered reference on chip). Terminal window shows UART output changes sinchronously with input sine amplitude (from +/-0V to +/-1.024V)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Another comment: it is not good idea to measure maximum and minimum voltage for AC amplitude measurement due to the inevitable noise contribution. Standard way extracting AC amplitude from single-frequency signal (such as AC mains) is to apply a Goertzel filter algorithm, many examples of which can be found online. Despite limited hardware options in PRoC 4100, it has fast and efficient CPU, which can handle such algorithm on-the-fly.
http://www.embedded.com/design/configurable-systems/4024443/The-Goertzel-Algorithm
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Odissey,
Thanks for kind comment. I have seen you selected in the ADC Block an external trigger HW which is driven by the pin 0_0. What should I connect to that pin? If I leave it open, then I get the same results as before. If I select free running in the ADC Block, then I get no answer at all from the UART Module. Just for your information, the ACS712 Module is delivering a signal between 0-5V with AC Mains Frequency (50 or 60Hz), I don't know if this can be a problem in the ADC Block as you selected Vinternal (1.024V) as Vref...
Can you help me here?
Thanks in advance,
Peter
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
peter,
The ADC is set to operate in external strobe mode to limit amount of isr calls to a meaningful amount. If left free-running, minimum amount of ADC data will be about 100k/sec, which is not possible to process. For 50/60 Hz AC, having 32 points per period is enough, so the trigger clock is set to 60x32~1.9kHz.
In P4 clock can not drive ADC directly, so standard procedure is to pass it through a pin to convert it to digital signal. Do not connect that pin, leave it open (you may check with a scope that signal).
First step would be is to run the project I supplied above and to observe it running properly with input AC signal in range 0 to 1V and offset 1.024 V and with UART output to terminal. Then modify it to suit you goals.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello odissey,
Thanks for the kind explanation. If I run your code just by changing the pinning to my PRoC, I get this UART output:
Ampl: 0 max: 2047 min: 2047
Ampl: 0 max: 2047 min: 2047
Ampl: 0 max: 2047 min: 2047
Ampl: 0 max: 2047 min: 2047
Ampl: 0 max: 2047 min: 2047
Ampl: 0 max: 2047 min: 2047
Are you sure your code works with the PRoC?
Which PSoC Creator are you using? As far as I remember my original code was working more or less fine with PSoC Creator 3.3 almost one year ago (at least it was not measuring always almost same min and max values).
I also tried with a PSoC4 and the CYBL-012011 and the result is always the same.
Looking forward to your feedback.
Peter
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
peter,
i suspect that the input pin is either not connected or fried. Try to change it to another pin. As you see from terminal window, there is small noise (~7) when sigmai is zero, but when pin is floating, then 2047 is what you will see.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Odissey,
I changed the pin and the result is the same, min and max are always 2047. I speeded up the oscillator of the pin and the same. I have never seen those min and max changing the value. I could make some parallel measurement with the scope and a DMM. Attached you can observe a screenshot with the scope, sorry it is very old and it has a lot of noise always. I am also performing measurements with a good DMM:
- When Vdd in PRoC= 4.5 and no AC is connected I measure 6mVrms (AC). This is the expected noise of the ACS chip at Vdd=4.5
- When Vdd in PRoC= 3.3 and no AC is connected I measure 6mVrms (AC). This is the expected noise of the ACS chip at Vdd=3.3
- When Vdd in PRoC= 4.5 and AC load of about 130mA is connected I measure a very fix value of 18mVrms (AC). It should be a difference between min and max of about 51. Following my calculations, this would be 125mA, what is more or less ok...
It must be something very basic in the configuration of the ADC or even in the PRoC, do you have an idea of what can be happening with all this new information?
Peter
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
odissey,
ADC is alive since I tested with the DieTemp Block and I got the temperature value correctly even when heating up and cooling down.
Coming back to this project, if I follow your recommendations and scale down the output of the sensor I will lost 2.5 sensitivity, what is not the goal of the project. Why I can not use the option VDD/2? I tried with that but it is not working either. Can you maybe simulate on your side with a waveform like the ACS712 (from 2 to 3V, for example) and send me the operating code? It would be perfect,
Thanks in advance,
Peter