Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Microcontrollers Forum Discussions

Browse the Community

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.

22391616 3976

PSoC™ 4

PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy

60343417 8973

PSoC™ 5, 3 & 1

The PSoC™ 5LP, PSoC 2 and PSoC 1 Forum discusses - 24-bit Digital Filter Block (DFB), 24 UDBs, DMA controller and integrating AFE, digital logic with user interface ICs with an Arm Cortex-M3 CPU solutions.

75253745 8707

CAPSENSE™ & MagSense

The Sensing Technology Forum discusses CAPSENSE™ - capacitive-sensing and MagSense inductive-sensing for consumer, industrial, automotive, and Internet of Things (IoT) applications.

991570 318

AURIX™

In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs

17209229 4537

TRAVEO™ T2G

Discussion forum regarding 32-bit TRAVEO™ T2G Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.

2504559 773

MOTIX™ MCU

The MOTIX™ MCU forum is designed for you to post your questions, comments and feedback about the famous Embedded Power ICs at anytime. Ask your technical questions or explore existing content!

4109145 641
filter icon

Featured Discussions

RuPi_283656
PSoC™ 5, 3 & 1
I'm trying to understand the USB setup. I have a board that has a USB connector connected to the DP and DM pins on the PSOC5.  I copied the code from ... Show More
yuhane
AURIX™
in TC38x,Can the local memory unit(LMU) and thre Distributed LMU (DLMU) as a whole LMU to be used in OVC function SAL-TC387QP-160F300S AD  Show More
SaGa_4641021
PSoC™ 6
Hi I am trying to create a simple program to read 10 bytes on UART through DMA and then write it again to the UART using DMA. I added blinking LEDs in... Show More
Adxi3
AURIX™
Hi.I'm a student. I have a PCB with the SAK-TC214L-8F133 chip on it. I would like to be able to connect to it using Memtool. I see Memtool supports th... Show More
ZJ01
AURIX™
Hi, I was recently working with TC387. I need to save some variables during standby mode, and after waking up, their value should not be initialized. ... Show More
Translation_Bot
MOTIX™ MCU
#include "tle_device.h " #include "eval_board.h " #include int main(void) { /* Initialization of hardware modules based on Config Wizard configura... Show More
kirankumar_infy
TRAVEO™ T2G
Hello, I am curious to know does IAR IDE, programmer tools support in Linux(Debian)OS. I know its not a right forum to ask here.  It would be really h... Show More
Darkalles
PSoC™ 4
Hi guys , I want to use freeRtos with psoc4 and my mcu is cy8c4248azi and I followed this guide : have a only one difference guide uses freeRtosV9.0.0... Show More
Wendy2
MOTIX™ MCU
大家好 : 关于ADC和DMA 有几个疑问,想得到帮助。 1.官方例程TLE9879_DMA_ADC1中,adc_ch_result[DMA_CH0_NoOfTrans]数组设置为8,但是IFXCONFIG里面,图1所示序列模式勾选了14个(7个通道+7个通道4重复采集),那么这个地方,DMA在传数... Show More
Guna
TRAVEO™ T2G

For 1 to 1 trigger ,SAR ch is decided based on logical channel or  ADC channel number?

Category Information

Microcontrollers

Discussions regarding PSoC and MCU products.