Microcontrollers Forum Discussions
Browse the Community
PSoC™ 6
Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.
PSoC™ 4
PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy
PSoC™ 5, 3 & 1
The PSoC™ 5LP, PSoC 2 and PSoC 1 Forum discusses - 24-bit Digital Filter Block (DFB), 24 UDBs, DMA controller and integrating AFE, digital logic with user interface ICs with an Arm Cortex-M3 CPU solutions.
CAPSENSE™ & MagSense
The Sensing Technology Forum discusses CAPSENSE™ - capacitive-sensing and MagSense inductive-sensing for consumer, industrial, automotive, and Internet of Things (IoT) applications.
XMC™
AURIX™
In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs
TRAVEO™ T2G
Discussion forum regarding 32-bit TRAVEO™ T2G Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.
MOTIX™ MCU
The MOTIX™ MCU forum is designed for you to post your questions, comments and feedback about the famous Embedded Power ICs at anytime. Ask your technical questions or explore existing content!
Legacy microcontrollers
Featured Discussions
1. Whether to use ADC or comparator for counter electromotive force
2. Is it only necessary to change the pole pair number to change the motor?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/motix-%E5%8F%8D%E7%94%B5%E5%8A%A8%E5%8A%BF-BLDC-BC-BEMF-EXAMPLE-TLE987X/td-p/744904
Show LessDear Team,
I want to know the difference between DAP miniwiggler and XMC_LINK_SEGGER_V1.
1.请问我在官网上看到了,伺服电机的方案。
2.请问这个方案是否开放?
3.如果开放能获得那些资料。
Whitepaper_CoolSiC™ – The_perfect_solution_for_servo_drives_EN (infineon.com)
Show LessHi Team,
In SDL example for cyt2cl CAN is initialized as CANFD. But, to configure it in Classical mode is there any specific register?
Thanks,
Pradeep
hi
i want to use the SCR in order to reduce the power consumption , and meet some block point. please check state flow bellowing :
if SW switch to SCR domain to execute, which position will sw execute next after wake up source login and exit from SCR domain ?
Step A (step A as the SW first code after reset )? or back to Step B?
Show Less
Hi,
I use the XMC4500F144K1024 chip as the main chip, and connect the TJAG download port of the slave ESP32 chip to the SPI pin of that chip. Is it feasible to use software to simulate SPI as a JTAG function and burn the program into the ESP32 chip? Is there any reference code or case for similar requirements that can be used for reference?
Thanks.
Show LessHello everyone! There are a couple of phenomena regarding the parameterization of the motor for actual debugging, and I'd appreciate any advice.
1. Startup duty cycle, more than 35% or more, a large number of tests, there will be a probability of power-on direct overcurrent protection, and then the system strike, restart to work properly;
2.Kp Ki parameter design, as if there is not much law, according to Kp/Ki = L / R, this formula does not seem to be very right, because in general, L is particularly small, so must be too large a difference, is not a 2:1 relationship, but at present the test to see how to set up, will only affect the corresponding speed, the motor running stability has not been found to have any effect. Regarding the pi parameter, if there is any opinion, please point it out.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/%E7%94%B5%E6%9C%BA%E5%8F%82%E6%95%B0%E8%AE%BE%E7%BD%AE/td-p/742823
Show LessHi,
I want to know CYT2B75CAE this controller is supporting AUTOSAR, If yes where i will get those information,
when i browse i am not able to find the information
Show LessHi team, I wanted to confirm whether the below EVM board is compatible for CY8CPROTO-063-BLE kit. If not can you share the correct EVM board details.
CY8CPROTO-063-BLE - Infineon Technologies
Thankyou
-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023