Nor Flash Forum Discussions
Hello
We are looking for top marking:
infineon S29GL256S90GHI010
infineon S25FL128SAGNFM000
Hi,
We are working on S70GL02GT11FHV010 NOR- Flash , in that we are tried to program the buffer ( i.e write to buffer , buffer to Flash using the commands) mentioned in the data sheet(page no-54) but we are failed to getting the correct answer.
Kindly help me to resolve this issue.
Thank you
Show LessHello need assistance on understanding which of the body markings is the date code for S29GL512T11DHIV10? TDS does not show correlation.
How to write onboard S70GL02GS12FHIV20?
Hello can I get a tds showing which markings on the component is the date code for S29GL512T11DHIV10
S29GL032A90TFIR40H product, it is old, can you tell me the MSL level?
Is it safe to assume that the GL-S series, for example, is MSL3, so is it 3?
Dear Temas,
Our customer asked the output setup time specification in S25FL128SAGMFIR13.
I have checked the datasheet, it only has the input setup time specification.
Our customer show us an IC specification, it has the same specification. It show the "write setup time".
Please help us to confirm it soon.
Thanks for your support.
Boris Su
Show LessHi, Our customer is looking for a successor to S29PL127J60TFI130.
But there is not writtern the explanation of Model Number 13 in the datasheet.
What is the Model number 13's property?
Regards, Shirakawa
Show LessHello,
I have an older product that uses the S25FL512SAGMFVR0.
VCC=3.3V and VIO=2.5V.
VCC and VIO ramp at the same time.
I have now seen failures with I/O pins IO1, IO2 and IO3.
That is the devices work in single and dual mode but not quad mode.
I have seen boards work either single or dual mode.
Replacing the parts does not fix the problem.
All board since built since 2015 with A on the third line work in quad mode.
SPANSION
FL512SAVFR1
823QQ015 A
All boards built after 2022 with B on the third line do not work in quad mode.
SPANSION
FL512SAVFR1
242QQ022 B
What is the difference between the parts A/B?
Any idea what could cause this problem/failure?
Regards Joe
Show LessHello,
Request you to provide me with the schematics and IBIS for Part No. S29JL064J70TF100