Announcements
IMPORTANT: Cypress Developer Community currently doesn’t allow sign-in to prepare for the upcoming transition. To learn more, check out our announcement.
cancel
Showing results for 
Search instead for 
Did you mean: 

Nor Flash

toyac_1469256
New Contributor II

Although the definition of the Typ value and the Max value is stated in Note 1, is it OK to say that it approaches the Typ value at 100,000 time P / E cycles and approaches the Max value at 1000,000 time P / E cycles ?

In Note 6, 100,000 cycles are stated as the Min value of the P / E cycle, but what problems will arise if it exceeds 100,000 times?

pastedImage_1.png

0 Likes
1 Reply
toyac_1469256
New Contributor II

While 100,000 cycles as guaranteed value, is not it strange that 1,000,000 cycles are subject to condition?

0 Likes