cancel
Showing results for 
Search instead for 
Did you mean: 

Nor Flash

JuBr_4604111
New Contributor

What is the maximum operation junction temperature for S29GL01GT11FHIV10?

What is the max power dissipation for S29GL01GT11FHIV10?

0 Likes
1 Solution
AS_36
Moderator
Moderator

Hi Juan,

You can calculate maximum operating junction temperature of our devices using below formula -

Tj = Theta Ja * P + Ta

Tj: Junction temperature

Theta Ja: Junction to ambient thermal resistance

P: Power consumption of the device (VCC (max) * ICC (max)).

Ta: Ambient temperature

Please see Theta Ja value for the requested device below -

Theta Ja: 39 °C/W

Maximum power dissipation: VCC(max) * ICC (max)

You can consider the Icc(max) value from the datasheet depending upon the operation being performed with the device.

Please let me know if you have any further queries.

Best Regards,

Apurva

View solution in original post

0 Likes
2 Replies
AS_36
Moderator
Moderator

Hi Juan,

You can calculate maximum operating junction temperature of our devices using below formula -

Tj = Theta Ja * P + Ta

Tj: Junction temperature

Theta Ja: Junction to ambient thermal resistance

P: Power consumption of the device (VCC (max) * ICC (max)).

Ta: Ambient temperature

Please see Theta Ja value for the requested device below -

Theta Ja: 39 °C/W

Maximum power dissipation: VCC(max) * ICC (max)

You can consider the Icc(max) value from the datasheet depending upon the operation being performed with the device.

Please let me know if you have any further queries.

Best Regards,

Apurva

View solution in original post

0 Likes
cono_285081
New Contributor

To get a more realistic power dissipation from the memory consider the dynamic power consumption when the memory chip is driving the IO. dynamic power = 0.5*C*V^2*F*No of IOs Total power is static+ dynamic. Below document has details. https://www.cypress.com/documentation/application-notes/an4017-understanding-temperature-specificati...

0 Likes