Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
BrLe_4684416
Level 1
Level 1

Hi,

We are currently experiencing high rates of data corruption in a CY15B104Q-LHXI device on our design.  We see corruption occur only when we write at a high temperature (up to +85C), power cycle and then read at low temperature (down to -40C).

Corruption appears to be at random locations in the device, and we see bits transition in both directions. The failure rate increases with the delta in temperature between write/read cycles.

We're currently investigating, and have started looking for potential reasons for the corruption.  We have a come across a few questions, would it be possible for one of the Cypress folks to take a look?

1. We find that if we replace the part with CY15Q102Q-S, OR FM25V20A the corruption does not occur. Are there any significant architectural differences between the 4Mb part and these 2Mb parts which may be causing the effect?

2. We have connected the centre pad to 0V on our design, although I noticed a note in the datasheet instructing it to be left floating. What are the implications of connecting this pad to ground?  Is this is possible reason for the corruption?

3. I have been looking at App notes AN304 and AN302, which give recommendations about holding chip select inactive during power transitions, and we are currently investigating this. However, I noticed that AN302 is marked as obsolete. What is the reason for that?  Is there any information in the note which is incorrect?

I'd be very interested to hear your thoughts, and know if you can suggest any reasons for the corruption.

Many thanks,

Bryan.

0 Likes
1 Solution
PradiptaB_11
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi,

Please find our comments below.

1) There is no significant architectural difference between the 4Mb and 2Mb parts.

2) The exposed pad on CY15B104Q-LHXI should not be soldered. Soldering the exposed pad will expose the F-RAM die to excessive heat, which may result in bit failures and margin loss. Hence it should be left floating without connecting to any pad on the PCB. Even the datasheet for FM25V20A recommends to not solder the exposed pad. Can you check for failure on another device without soldering the exposed pad?

3) The issue mentioned in App note 302 is no longer applicable for FRAM parts as the parts with these issue were obsoleted and no longer available. The app note was anyways not applicable for CY15B104Q.

Fixing the issue should resolve your issue, if you have any further concerns you can let us know.

Thanks and Regards,

Pradipta.

View solution in original post

0 Likes
3 Replies
PradiptaB_11
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi,

Please find our comments below.

1) There is no significant architectural difference between the 4Mb and 2Mb parts.

2) The exposed pad on CY15B104Q-LHXI should not be soldered. Soldering the exposed pad will expose the F-RAM die to excessive heat, which may result in bit failures and margin loss. Hence it should be left floating without connecting to any pad on the PCB. Even the datasheet for FM25V20A recommends to not solder the exposed pad. Can you check for failure on another device without soldering the exposed pad?

3) The issue mentioned in App note 302 is no longer applicable for FRAM parts as the parts with these issue were obsoleted and no longer available. The app note was anyways not applicable for CY15B104Q.

Fixing the issue should resolve your issue, if you have any further concerns you can let us know.

Thanks and Regards,

Pradipta.

0 Likes

Hi Pradipta,

Thanks for your reply, much appreciated. We’ll try some experiments to see if this fixes the problem.

Just trying to understand the issue further, am I right in saying that the device can get damaged during the soldering process? We use vapour-phase soldering, where the whole device should get to an even temperature – are there any restrictions on using vapour-phase reflow for this device?

Also, if the problem is purely to do with heat damaging the device, am I right in saying that there are no electrical effects of connecting the central pad? Our PCB footprint has a corresponding pad I’m wondering if removing the solder paste from the pad before reflow would be an acceptable solution. This way, there will be no soldered connection and therefore less heat transfer, but there will still be an electrical connection. Is this acceptable?

I guess I’m wondering about the purpose of the pad on the device.

Thanks again for your help,

Bryan.

0 Likes

Hi Bryan,

Please find my comments below.

The purpose of the pad on the device is that Standard QFN or DFN package has always been with exposed pad for thermal performance. If it was design without exposed pad, it would be a custom leadframe/package. We do not want to offer a custom QFN/DFN package with unproven manufacturability and reliability. So we have a DFN package with note says that EXPOSED PAD should not be soldered.

Our QTP (qualification) data is based on the use of convection solder reflow ovens (and not vapor phase solder reflow ovens). So unfortunately,  we don’t have any data to answer your question on this.

DO NOT Design any land pattern on the PCB (Definition of the package in the library)  -> the stencil will have no "window", no solder paste will be present -> no soldering of the exposed PAD to the PBA at all -> no risk of contact to any land pattern.

Thanks,

Pradipta.

0 Likes