cancel
Showing results for 
Search instead for 
Did you mean: 

Non Volatile RAM (F-RAM & NVSRAM)

NaMo_1534561
Contributor II

Hello,

Could you provide AC Switching Characteristics of I2C standard mode (100KHz) of FM24V01A?

Datasheet shows the Fast mode plus(1MHz) and the Hs mode(3.4MHz) only.

I believe that it is same as I2C bus specification published by NXP.

Customer want to confirm some parameters which are defined as max value at the standard mode.

Best Regards,

Naoaki Morimoto

0 Likes
1 Solution
PradiptaB_11
Moderator
Moderator

Hi Naoaki-san,

Yes, you are correct the specs are same as I2C bus specification by NXP. I am attaching the user guide by NXP which has the specs defined in it. Kindly refer to it, and let us know if you have any further query.

https://www.nxp.com/docs/en/user-guide/UM10204.pdf

Thanks and Regards,

Pradipta.

View solution in original post

0 Likes
1 Reply
PradiptaB_11
Moderator
Moderator

Hi Naoaki-san,

Yes, you are correct the specs are same as I2C bus specification by NXP. I am attaching the user guide by NXP which has the specs defined in it. Kindly refer to it, and let us know if you have any further query.

https://www.nxp.com/docs/en/user-guide/UM10204.pdf

Thanks and Regards,

Pradipta.

View solution in original post

0 Likes