Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

ModusToolbox™ Forum Discussions

Sort by:
Lance
ModusToolbox™
Hi infineon Team, A few days ago, ModusToolbox can still open normally, but today the following problems occur, how to solve. ERROR:there was an error... Show More
gargosuman
ModusToolbox™
When I try to create a new project with Project Creator I get an error getting device_db:     I have all the environment variable set up as suggested... Show More
SaAo
ModusToolbox™
Hello, The following error occurred when HelloWorld was created with NewApplication in ModusToolbox.No space is used.Could you identify the cause of t... Show More
Panometric
ModusToolbox™
I have a need to generate 3 or more target programs from almost the same code base. However: design.modus must be different some preprocessor DEFINES... Show More
avra
ModusToolbox™
Problem:The Device Configurator is showing wrong frequency for CLK_TIMER. Source of CLK_TIMER is set to IMO with 8MHz frequency. But the frequency of ... Show More
Translation_Bot
ModusToolbox™
The templates that can be selected for Modus's new PSoC6 project are all PSoC62/63/64 series. How can I build a new PSOC61 project  smartconx_target@... Show More
jvavra_UICO
ModusToolbox™
I understand optimization must be set in the project makefile using the CFLAGS option. However, when comparing optimization off (-O0) to optimization ... Show More
YR1
ModusToolbox™
in wiced_hal_pspi.h #define wiced_hal_pspi_init wiced_hal_pspi_init_patch void wiced_hal_pspi_init_patch(UINT8           devRole,                    ... Show More
jsmith678x
ModusToolbox™
I'm trying to use the POSTBUILD section in the Makefile. It seems I have no any path variable here so I have defined my toolchain path and project pat... Show More
AndreasHB
ModusToolbox™
I would like to edit my project on a network drive. When I create a new project, I get the following error message: [1]: there was an error retreiving... Show More