MOTIX™ SBC

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
EvelineP
MOTIX™ SBC
VSINT supplies the SBC functions, in particular the voltage regulator VCC1, which is intended to supply the microcontroller VS supplies the gate driv... Show More
User22801
MOTIX™ SBC
The gain drift is the drift of the gain after calibration.For example, the gain of the current sense amplifier is calibrated at 25 °C with a two point... Show More
User22801
MOTIX™ SBC
In general, it is recommended to connect unused WKx pins to GND.However, it is possible to leave the unused WKx pins floating, as long as the internal... Show More
User22801
MOTIX™ SBC
What is the max. possible capacitance values of CCP, CCP1, and CCP2 for the TLE9210x device family?CCP1 is an external capacitor connected between CPC... Show More
User22801
MOTIX™ SBC
Is it okay to put 100nF at each SHx pin for the ECU level ESD protection? Are there any concerns for over-current detection / drain-source overvoltage... Show More
User22801
MOTIX™ SBC
When are the external high-sides / low-sides turned on after a drain-source overvoltage detection?When the status bits HSxDSOV or LSxDSOV are cleared,... Show More
User22801
MOTIX™ SBC
When a half-bridge is configured as Active OFF (HBxMODE[1:0] = 11B while the charge pump is enabled), then the MOSFETs of HBx are indeed actively tur... Show More
User22801
MOTIX™ SBC
Why is the gate of the high-side MOSFETs at the VS potential when the half-bridge is off?When a half-bridge is configured as Active OFF (HBxMODE[1:0] ... Show More
User22801
MOTIX™ SBC
The active free-wheeling reduces the power losses in the free-wheeling MOSFET during the PWM operation (pulse width modulation), therefore reducing co... Show More