MADK

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
User22872
MADK
In PFC stage of EV charger. How to calculate the maximum PI output value for pi voltage controller if the required power limit is 3.4kW. This value is... Show More
User19250
MADK
Hi,1. Does REF-AIRCON-C302A-IM564 have a wizard configuration file that goes with IMC302A-F064? Where can I find it?2. Is there any CAN-Bus example fo... Show More
Rakesh_rp
MADK
I am using  xmc1300 development board for PFC stage in 3.4kW onboard EV charger. In the software for PI  voltage control loop I have to set the max po... Show More
User22853
MADK
Hello Team,Please let me know how to rotate the BLDC motor using sensored algorith.I have done the sensorless rotation. Need to switch to the sensored... Show More
User17471
MADK
How could I measure Initial angle by hall sensor and use it?I have a problem with IMC101. When i'm trying to use sensorless pmsm with InitialSense som... Show More
User21557
MADK
DFP for IMC in KEILHiIm working by IMC300A and need to write my code in KEIL IDE so I need download firmware pack(DFP) to add in Keil packin " AN2020_... Show More
User21557
MADK
HiIm working by IMC300A and need to write my code in KEIL IDE so I need download firmware pack(DFP) to add in Keil pack in " AN2020_10 IMC300A periphe... Show More
User20357
MADK
IMC101-T04I need to get absolute MOTORCUURENT and MOTORVOLTAGE.How can I get scale factor by reading regsters ONLY. --External software does not know ... Show More
User19585
MADK
Hello everyone,I am using a IMM101T and I am controlling it via UART.It is working, but there is a part of the communication that is not working as st... Show More
User19741
MADK
I’ve got a serious problem with a IMC101 implementation.We’ve been using a IMC101 in one of our products for a while now, and it’s been working ok for... Show More