Legacy microcontrollers Forum Discussions
Now Making...
--------------------Configuration: IS12.prj - Debug--------------------
InitManage.c
*** .\Driver\_ffmc16.h(16) E4077P: #error "The I/O register file of the specified CPU option does not exist"
*** .\Driver\_ffmc16.h(16) E4077P: #error "The I/O register file of the specified CPU option does not exist"
main.c
*** .\Driver\_ffmc16.h(16) E4077P: #error "The I/O register file of the specified CPU option does not exist"
*** .\Driver\_ffmc16.h(16) E4077P: #error "The I/O register file of the specified CPU option does not exist"
TaskManage.c
*** .\Driver\_ffmc16.h(16) E4077P: #error "The I/O register file of the specified CPU option does not exist"
*** .\Driver\_ffmc16.h(16) E4077P: #error "The I/O register file of the specified CPU option does not exist"
_ffmc16.c
*** d:\work\seat\source\cs95msm\driver\_ffmc16.h(16) E4077P: #error "The I/O register file of the specified CPU option does not exist"
VCT.c
*** d:\work\seat\source\cs95msm\driver\_ffmc16.h(16) E4077P: #error "The I/O register file of the specified CPU option does not exist"
RLT.c
*** d:\work\seat\source\cs95msm\driver\_ffmc16.h(16) E4077P: #error "The I/O register file of the specified CPU option does not exist"
*** d:\work\seat\source\cs95msm\driver\_ffmc16.h(16) E4077P: #error "The I/O register file of the specified CPU option does not exist"
ADC.c
can you tell me why ? thanks! F2MC-16 Family SOFTUNE Workbench V30L35; MB96F646R MCU
Show LessHello Community,
I'm reading this document:
Microsoft Word - mcu-an-300213-e-v13-16fx_flash_security.doc (fujitsu.com)
In section 2.1 the document sais:
'[...] If the supplied Unlock Key is all 0, the Flash Security cannot be disabled at all.'
My question is: If I set the Unlock Key fully with zeros, then will I be able to perform a Chip Erase with the CYPRESS FLASH MCU Programmer after this full-zero setting is applied?
Thank in advance,
Gabor
Show LessHi, I am about to connect a Touchscreen which uses CYTMA568 through I2C to a custom carrier board with NXP iMX6 Application processor.
The linux is built with openembedded / yocto project (dunfell branch) and uses a customized device tree.
First, the BSP provided by the SoM Manufacturer (Toradex, SoM is Colibri iMX6DL), didn't provide support for this touch controller.
I found the following patch series to add the driver:
https://lwn.net/ml/linux-kernel/20180703094309.18514-1-mylene.josserand@bootlin.com/
I also added a node in device-tree according to the binding documentation like this:
&i2c3 {
status = "okay";
[...]
cyttsp: cyttsp@24 {
compatible = "cypress,cyttsp5";
reg = <0x24>;
interrupt-parent = <&gpio7>;
interrupts = <10 IRQ_TYPE_LEVEL_LOW>;
touchscreen-size-x = <800>;
touchscreen-size-y = <480>;
status = "okay";
};
};
I get the following errors during boot:
[ 0.394465] cyttsp5 1-0024: Error on deassert int r=-22
[ 0.399802] cyttsp5 1-0024: Fail initial startup r=-19
I can use i2cdetect and i2cread to access the device, but the touch driver isn't loaded properly.
Show Less
Hello,
I would like to use a 4MHz ceramic resonator as an external oscillator for FM3 MCU (CY9AF144NAPMC-G-MNE2).
Are there any documents that explain the matching characteristics of oscillation circuits, design guides, or other design methods?
Regards,
Shimamura
Show LessI want to program the MB91F467D in the circuit, the script asks for MD0; MD1e MD2 connected to Vss pin 73 reset SOT4 and SIN4 plus Vcc more of the error. Is there anything I can do to program it? Thank you for your attention.
Show LessHi.
My customer wants to use CY95F334KT PMC-G-UNE2.
My customer used CY95F334KT PMC-G-SNE2
CY95F334KTPMC-G-SNE2
CY95F334KTPMC-G-UNE2
Can the above two be considered equivalent products?
Is it okay to think that the specifications are the same due to differences in processes, etc.?
Best Regards.
Show Less
What is the RAM save voltage and RAM clear voltage of the microcontroller?
Also what happens when the VCC falls below the operating threshold? How is the memory management done? Show Less