Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Delmore
Level 2
Level 2
Distributor - Arrow(GC)
10 replies posted 25 sign-ins 5 questions asked

At 9V, the PWM driver will see the LED flicker that can be recognized by human eyes. When testing the waveform with the oscilloscope, it is found that the power supply voltage is forcibly pulled down by a few tenths of a volt. When the voltage is adjusted to 10V or above, the flicker disappears, but the phenomenon of forcibly pulling down the power supply detected by the oscilloscope still exists.

This phenomenon is especially obvious when multiple devices supply power at the same time. The waveform of tail point is as follows. Please help analyze whether this phenomenon is normal and what causes it.

Delmore_2-1652925182547.png

 

Delmore_0-1652925124705.pngDelmore_1-1652925152731.png

 

0 Likes
2 Replies
Kanahaiya_K
Moderator
Moderator
Moderator
50 likes received 100 solutions authored 10 likes given

Hello @Delmore 

Thanks for posting on the Infineon Developer Community.

Can you please clarify the following points?

Please share the complete schematics along with the point where you are measuring the waveform? Since ,I am not able to find the tail point in the complete schematics.

 

Regards

Kanahaiya

0 Likes
Kanahaiya_K
Moderator
Moderator
Moderator
50 likes received 100 solutions authored 10 likes given

Hello,

Please refer to the following thread link for more details. 

https://community.infineon.com/t5/LITIX-Automotive-LED-Driver-IC/TLD2141-3EP-LED-flicker-and-power-s...

Regards
Kanahaiya

0 Likes