公告

大中华汽车电子生态圈社区并入开发者社区- 更多资讯点击此

Tip / 登入 to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
jimmy-gao123
Level 1
Level 1
First question asked Welcome!

我的尾灯项目,tail 电流需要3mA,不过我看规格书输出 是5.62~72mA, 配合PWM 做到3mA,请问这种情况下精度怎么样

0 点赞
1 解答
Klaus_Ma
Moderator
Moderator
Moderator
100 sign-ins 50 solutions authored 50 replies posted

Hello ,

这颗芯片输出电流5.62~72mA,TJ= 25°C电流精度±5%。但是在全范围温度下,低电流工况精度±10%.

如果通过外部PWM控制实现3mA输出电流,抛开可行性问题,电流精度要超过±10%了,而且更多的是由PWM方案决定,无法给出一个准确范围。

在原帖中查看解决方案

1 回复
Klaus_Ma
Moderator
Moderator
Moderator
100 sign-ins 50 solutions authored 50 replies posted

Hello ,

这颗芯片输出电流5.62~72mA,TJ= 25°C电流精度±5%。但是在全范围温度下,低电流工况精度±10%.

如果通过外部PWM控制实现3mA输出电流,抛开可行性问题,电流精度要超过±10%了,而且更多的是由PWM方案决定,无法给出一个准确范围。