cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Working of the PSoC® 3/5LP RTC Without a Power Supply and Across Resets – KBA93082

KishoreS_96
Employee

Working of the PSoC® 3/5LP RTC Without a Power Supply and Across Resets – KBA93082

Version: **

Translation - Japanese: PSoC ® 3/ 5LP RTC 無電源時およびリセット前後の動作 - KBA93082 - Community Translated (JA)

Question: Can the PSoC® 3/5LP real-time clock (RTC) run without a power supply or across resets (that is, no change even if PSoC 3/5LP is reset)?

Answer:

The PSoC 3/5LP RTC block requires a constant power supply. There is no internal capacitor to hold some charge for keeping the RTC running for some time without a power supply. The RTC can run in sleep mode and alternate active mode. In this case, one pulse-per-second (OPPS) has to be the wake-up resource to update real-time for the clock. The RTC cannot run in hibernate mode.

Once PSoC 3/5LP is reset, the RTC block will also get reset and it will start from the beginning.

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Dec 19, 2011 03:12 AM
Updated by:
 
Contributors