cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

VDAC output in 4V mode when PSoC 3/5 is operating at 3.3V

Anonymous
Not applicable

VDAC output in 4V mode when PSoC 3/5 is operating at 3.3V

Question: If PSoC 3/5 is running at 3.3 V and VDAC is running in 4 V mode, what will be the expected output?

 

Answer:

Irrespective of the operating voltage, step size will be the same. But output will saturate at about Vdda – 100mV.
 

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Mar 14, 2011 05:15 PM
Updated by:
Anonymous
 
Contributors