Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Type of Xtal used for ECO in TRAVEO™ II Family

Type of Xtal used for ECO in TRAVEO™ II Family

IFX_Publisher1
Community Manager
Community Manager
Community Manager
250 sign-ins First comment on KBA 250 replies posted

Crystal Unit and Ceramic Resonator can be used for ECO. TRAVEO™ II has a built-in ECO gain control amplifier and can support various Xtals by setting the amplifier parameters.

Amplifier parameters are calculated using the specifications of Xtal. For more details, see the “Clocking System” section of the Architecture Technical Reference Manual and the ECO User Guide. If the calculation result of an Xtal is out of the specified range, the corresponding Xtal cannot be used.

Note: This applies to the following series of TRAVEO™ II MCUs:

  • CYT2 Series
  • CYT3 Series
  • CYT4 Series
0 Likes
105 Views