Switching VDDL for CY22395
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Answer:
There are side effects of switching the VDDL between 2.5V and 3.3V. We have default output drive settings for 2.5V ([10]=M High) and 3.3V ([01]=M Low). If the device is programmed for 2.5V outputs, when VDDL is powered with 3.3V, the outputs will be driven a little harder with faster edge rates. The reverse will be true as well, if the outputs are programmed for 3.3V. In this case, when VDDL=2.5V, the outputs will be driven a little weaker and edges will be slowed down. The datasheet specifications on edge rates and IOH/IOL are based on the default output drive settings. Jitter may or may not be affected, increased edge rates could help lower jitter due to the increased rate through the threshold region, but then again you could have increased noise due to the higher edge rate which could increase jitter as well.
- Tags:
- clock generation
-
This widget could not be displayed.Anonymous