cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Setup Time & Skew violation warning messages (STA) for a SPI based PSoC Creator project

KishoreS_96
Employee

Setup Time & Skew violation warning messages (STA) for a SPI based PSoC Creator project

Answer:

Question: I'm getting around 33 warning messages when I compile a SPI based project in PSoC Creator. How to resolve them?

Response:

Following are the format of warning messages you might be getting:

sta.M0012: Setup time violation from clock "clock1" at "register1" to clock "clock2" at "register2".

sta.M0010: The skew from clock "clock1" at "register1" to clock "clock2" at "register2" is "time1" ns. The skew is too large for a clock with period "time2 (< time1)" ns.

Please check whether you have uncheked the "Clock Synchronization" for SPIM & SPIS input pins. You might see these warning messages because of this.

  

This uncheking has to be done for all the input pins - MISO (SPIM) & MOSI, SCLK, SS (SPIS)

Note: If you getting any STA warning message related to asynchronous nature, Please refer to this KB.

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Jun 23, 2011 12:35 AM
Updated by:
 
Contributors