SLRD/SLWR Pins During GPIF Mode of FX2LP
Anonymous
Not applicable
Jun 13, 2011
12:35 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Jun 13, 2011
12:35 AM
During GPIF burst transaction, is the GPIF in control of the SLWR, SLOE signals internally? Do you need to tie the appropriate CTLx output signals to these signals?
The SLWR, SLRD, SLOE pins are only active when FX2LP is configured in Slave FIFO mode. These pins assume a different functionalities when FX2LP is not operating in Slave FIFO mode. For example, when configured in GPIF mode, the SLRD and SLWR lines are replaced with RDY0 and RDY1 lines respectively.
Translation - Japanese: FX2LPのGPIFモード中のSLRD / SLWRピン - Community Translated (JA)
Rate this article: