Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

S6BT112A CXPI Transceiver: Sleep Mode Behavior for Slave Node - KBA223646

S6BT112A CXPI Transceiver: Sleep Mode Behavior for Slave Node - KBA223646

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Version: **

Translation - Japanese: S6BT112A CXPIトランシーバー:スリープモード時のスレーブノードの動作 - KBA223646 - Community Translated (JA)

Question:

When data is received during Sleep mode at the Slave node, what kind of signal is output to the pins?

Answer:

  • The signal of BUS pin is output to the CLK pin without decoding when in Sleep mode at the slave node. If this signal is input to the INT pin of the connected MCU, it can be used as the wakeup signal of the connected MCU.
  • The RXD pin is fixed at "H" level.
252 Views
Contributors