cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

S6BP501AおよびS6BP502AのLX5VピンのAC定格 - KBA227095 - Community Translated (JA)

SivaK_96
Employee

S6BP501AおよびS6BP502AのLX5VピンのAC定格 - KBA227095 - Community Translated (JA)

Community Translated by NoTa_4591161        Version: **

Translation - English: AC Rating of LX5V Pin of S6BP501A and S6BP502A - KBA227095

質問:

S6BP501AおよびS6BP502ALX5VピンのAC定格はどのくらいですか?

回答:

1S6BP501AおよびS6BP502ALX5Vピンのスイッチング波形の例を示します。

1. LX5Vスイッチング波形の例

pastedImage_0.png 

LX5V端子のAC耐電圧は12 Vですので、1ようなリンギング波形が発生してもICは破壊されません。

高周波リンギング波形を正しく測定するには、ICピンの近くで測定します。また、2示すように、オシロスコープのプローブのGNDを短絡して接続する必要があります

2. オシロスコーププローブGND

   Capture.JPG

リンギングノイズを低減する方法として、スナバ回路を追加する方法があります。3スナバ回路の例を示します。

3. DD5Vのスナバ回路の例

pastedImage_18.png​ 

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Jul 13, 2020 12:52 AM
Updated by:
 
Contributors