cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Running the debugger on a custom board without external memory AN2131

Anonymous
Not applicable

Running the debugger on a custom board without external memory AN2131

Question: Is it possible to run the debugger on the AN2131S, since it does not have external memory?

 

Answer:

We include an internal version of the monitor with the development kit. However, with no external memory available you will be limited by the amount of remaining memory.

There is a readme.txt file in the C:\cypress\usb\target\monitor that explains the various monitors and the resources used by them.

There are some places where you can reclaim some RAM for your application. First, there is a chunk of code in main () that can be removed if your descriptors are located in internal RAM. You can remove this entire if statement:

if ((WORD)&DeviceDscr & 0xe000)
{... }


Also, if your device is self-powered, it does not need to worry about suspend and resume and you can remove the entire if statement:

if (sleep)

{ ... }

(ISODISAB bit in ISOCTL), and unused bulk endpoint buffers for code and data.

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Dec 19, 2008 12:00 AM
Updated by:
Anonymous
 
Contributors