Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

RESET vs. CLK (CY7C68000).

RESET vs. CLK (CY7C68000).

Anonymous
Not applicable
Question: Is there a way to keep the CLK output running when the RESET input is asserted? If not, what is the maximum time from the de-assertion of RESET until the CLK output is stable again?

 

Answer:

When asserted the "Reset" pin is hardware reset for the chip. There is no way to keep the "CLK output" running during the power-up sequence of the device. The internal PLL stabilizes approximately 200 us after VCC has reached 3.3V (CY7C68000 Datasheet, Page 5 of 17, section 3.4). When using a crystal, the minimum reset time (tRESET) is 1.9 ms. (CY7C68000 Datasheet, page 12 of 17, Table 8-1). TX2 is currently obsolete,  the functional replacement is TX2UL. All the related collaterals of TX2UL can be found in the link here.

0 Likes
275 Views
Contributors