Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC 6 BLE: Peripheral Updating Connection Parameters

lock attach
Attachments are accessible only for community members.

PSoC 6 BLE: Peripheral Updating Connection Parameters

Yugandhar
Moderator
Moderator
Moderator
1000 replies posted 5 likes given First comment on blog

The project attached below shows how to update the Connection Parameters in a BLE connection using the PSoC 6 BLE device. Peripheral device can update the connection parameters by sending a Connection Parameter Update Request packet to the Central device. In this project, once the device connects to a peer device, a Connection Parameter Update Request can be sent from the GAP Peripheral when the user presses the switch (SW2) on the kit.

Schematic Diagram:

Yugandhar_0-1631772056682.png

 

Hardware Required: CY8CKIT-062-BLE PSoC 6 BLE Pioneer Kit

Software Required: PSoC Creator™ 4.4, CySmart 1.3, Serial Terminal application (like TeraTerm)

PSOC Creator project and project datasheet are attached below.

Attachments
0 Likes
749 Views