cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

PCMCIA Implementation for the CY7C68013/CY7C68013A (FX2/FX2LP)

Anonymous
Not applicable

PCMCIA Implementation for the CY7C68013/CY7C68013A (FX2/FX2LP)

Question: Can the FX2/FX2LP be used to implement a PCMCIA controller? If so, are there any reference designs or application notes that explain how to do this?

 

Answer:

Yes. The FX2 can be used to implement the PCMCIA controller. Currently, we do not have any examples or collateral that provide a starting point to implement this. But this can be implemented using the GPIF feature of the FX2.

The FX2 has a feature called the GPIF (The General Programmable InterFace ) which is an extremely flexible 8- or 16-bit parallel interface that can provide a glueless interface between the EZ-USB FX2 and many different types of external peripherals. The GPIF allows the EZ-USB FX to perform local bus mastering to external peripherals using a wide variety of protocols. More information about GPIF can be found in the link EZ-USB® FX2LP™ GPIF Design Guide - AN66806

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Apr 03, 2011 02:21 PM
Updated by:
Anonymous
 
Contributors