Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

OptiMOS™ 5: When to use TOLT devices over traditional TOLL devices?

OptiMOS™ 5: When to use TOLT devices over traditional TOLL devices?

IFX_Publisher2
Community Manager
Community Manager
Community Manager
1000 replies posted First like given 750 replies posted

Community Translation: OptiMOS™ 5: 従来のTOLLデバイスではなく、TOLTデバイスを使用するのはどんな場合か?

Traditional TOLL packages are rated up to 300 A, equivalent to TOLT. However TOLL devices dissipate heat through the PCB, which has the heatsink mounted underneath. This limits the thermal performance and power handling ability of the system. TOLT devices overcome this limitation with top-side cooling, thereby allowing the customer to achieve higher power capability.

0 Likes
141 Views