Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Message 'Could not connect to ICE'

Message 'Could not connect to ICE'

Anonymous
Not applicable
Question: When I try to run the drawusb project I get a "Could not connect to ICE" message.  How do I resolve this?

 

Answer:

The Project settings in the PSoC Designer tools default to having the ICE connected to LPT1.  To connect to the ICE via USB:

1.  Select Project from the top menu

2.  Select Settings

3.  Select the Debugger tab

4.  From the ICE connected to: drop down menu select USB/0413D324, then press OK. Note: USB/0413D324 reflects an unique ICE number, your actual number will differ from what is shown here.

bha05040701

0 Likes
238 Views
Contributors