cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Manufacturing mode in CY4611B(FX2LP-to-ATA/ATAPI reference Design)

Anonymous
Not applicable

Manufacturing mode in CY4611B(FX2LP-to-ATA/ATAPI reference Design)

Question: What is Manufacturing mode in CY4611B how is detected and handled inside the firmware?

 

Answer:

In Cy4611B the firmware can boot through I2C based EEPROM. Prior to that  the combined file of the Firmware (CY4611. hex)and EEPROM configuration file (.iic)  must be  stored in the EEPROM memory ( (0x0000-0x3eff)-Cy4611.hex  and (0x3f00-0x3fff)-EEPROM Configuration file(.iic) ).This EEPROM configuration file contains different parameters related to ATA/ATAPI compliant devices. Once the firmware boots from EEPROM during the initialization sequence if the ATA_RESET#(Pin 1) and DD#7(pin 3) pins on the40-pin ATA connector are shorted then AT2LP will enter  manufacturing mode.

Following is the piece of code inside CY4611B firmware to detect a short b/w  RESET# and DD7 pins

            if (!ATAPI_RESET_)

               {

               OEB = 0x80;

               PB7 = 0x80;

               if (ATAPI_RESET_)

                  enterMfgMode();

               OEB = 0x0;

               }

As per the above code is the ATA_RESET# signal is in a low state then  DD7 is  driven high and ATA_RESET# signal is cross-checked to verify if that pin also senses high and if true it eventually indicates a short.Then CY4611B enters manufacturing mode. This will completely stop the initialization of ATA/ATAPI device connected to the 40-pin bus . The  parameters  of the EEPROM configuration file(.iic) can then be modified and then re-programmed (to suite several types of ATA/ATAPI devices) using a Blaster software tool  available in the CY4611B kit software.

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Jan 03, 2011 08:06 AM
Updated by:
Anonymous
 
Contributors