Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Lattice Crosslink FPGA configuration and UVC Color bar video streaming using Cypress FX2LP – KBA30768

lock attach
Attachments are accessible only for community members.

Lattice Crosslink FPGA configuration and UVC Color bar video streaming using Cypress FX2LP – KBA30768

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Translation - Japanese: サイプレスFX2LPを使用したラティスクロスリンクFPGA構成とUVCカラーバービデオストリーミング – KBA30768 - Community Translated (JA)

Version: **

This KBA documents the details about implementation of FPGA configuration and UVC framework on FX2LP firmware. It uses Lattice Crosslink FPGA to generate and stream color bar video. The firmware example attached with this KBA binds with the standard UVC driver of the Host PC / mobile phone. The color bar is generated on FPGA and streamed by FX2LP firmware. The firmware is tested using FX2LP Low Cost Board (Figure 2) and MIPI Camera Crosslink FPGA Addon Board (Figure 3). The following block diagram shown in Figure 1, provides an overview of the high-level design of interfacing a camera using FX2LP and Crosslink FPGA.

Figure 1. System Block Diagram

pastedImage_6.png

Figure 2. FX2LP Low Cost Board

pastedImage_12.png

Figure 3. MIPI Camera Crosslink FPGA Add-on Board

pastedImage_13.png

FX2LP Firmware features

This firmware consists of slave FIFO interface, UVC framework and Vendor class interface to support FPGA configuration and video streaming. UVC framework used in this project is described in Cypress Application note AN75779. Please note that this application note implements USB Video Class (UVC) Framework for an FX3 device. But this can be used as a reference for understanding the details about UVC framework.

This firmware supports video streaming in YUY2 format with 640 x 480 resolution. The slave FIFO interface of the FX2LP device gets the  640 x 480 resolution color bar video from the FPGA and loads it onto FX2LP’s FIFO buffer. FX2LP sends this video data to the host over the UVC interface. UVC-related requests and enumeration are handled by the FX2LP device. Crosslink FPGA starts streaming according to FIFO buffer empty control signals sent from FX2LP.

The USB Endpoint 2 (EP2) size is configured as 512 bytes, quad buffered to function as a Slave FIFO Bulk IN receiver. Flag A is configured as FIFO empty flag signaling Crosslink FPGA to begin loading data onto buffer and FLAG B is configured as FIFO full flag. FPGA asserts PKTEND signal to send short packet data of 1280 (640 x 2) bytes to send one line of video stream, buffer is loaded again when empty flag is asserted and  UVC request reads and clears data in EP2.

Crosslink FPGA is configured (programmed) via I2C by FX2LP. FX2LP receives bitstream from PC through vendor class interface as vendor commands. Vendor commands use control endpoint to receive the bitstream data. A custom vendor class host application is built and provided along with this KBA which takes in generated FPGA bitstream and breaks it into multiple blocks of 4096 bytes and transmits it repeatedly as a vendor request. Commands to configure and write to Crosslink FPGA over I2C has been implemented and can be found in td_init() function. FX2LP switches to Slave FIFO upon assertion of CDONE from Crosslink indicating completion of FPGA configuration.

Latest revision of MIPI Camera Crosslink FPGA Add-on Board includes an I2C - 2Mbit EEPROM, which can be used to load the bitstream directly to FPGA. This will eliminate the need to download bitstream from HOST PC to Crosslink every time device is reset. This hasn’t been tested and will be updated accordingly.

Testing the Implementation

The attached project includes Crosslink FPGA code, which implements a color bar video generation and stream using FX2LP’s slave FIFO Master interface. YUY2 640 x 480 video resolution was streamed with a 12 MHz[NB1] clock, leading to data speed of 192 Mbps (12M X 16 bits). This was tested on FX2LP Low cost board, schematic files for which can be found on KBA229176 and MIPI Camera Crosslink FPGA Add-on Board, schematic files of this board is attached with this KBA. The UVC application used to stream video color bar is MPC-HC video player. Generated color bar with rendering statistics are as shown in Figure 4.

Figure 4. Streamed YUV Color bar
pastedImage_26.png
Pin Mappings made for this implementation as per Table  1.
Table 1. Pin Mapping

Serial number

Signal Name on MIPI Camera Crosslink FPGA ADD-ON Board

FX2LP PIN Name

1

PA0

PA0

2

SLWR

SLWR

3

PKTEND

PA6

4

FLAG A

CTL0

5

FD0

PB0

6

FD1

PB1

7

FD2

PB2

8

FD3

PB3

9

FD4

PB4

10

FD5

PB5

11

FD6

PB6

12

FD7

PB7

13

FD8

PD0

14

FD9

PD1

15

FD10

PD2

16

FD11

PD3

17

FD12

PD4

18

FD13

PD5

19

FD14

PD6

20

FD15

PD7

21

ADR0

PA4

22

ADR1

PA5

23

CDONE

PA1

24

CRESET

PA3

Additional Modifications Possible

You can further modify the attached firmware to include more resolutions, formats, and frame rates. You can also add standard UVC video controls and custom extension unit controls.

“MIPI CAMERA FPGA ADD-ON BOARD FOR FX2LP” also has an image sensor connector and an image sensor module can be connected to stream video instead of color bar.

Files enclosed along with KBA

  1. “MIPI CAMERA FPGA ADD-ON BOARD FOR FX2LP” Schematic
  2. Crosslink FPGA logic project files
  3. FX2LP firmware project files
  4. Custom Application to send Generated Bitstream over Control Endpoint to FX2LP
Attachments
0 Likes
1438 Views
Contributors