Announcements
IMPORTANT: Cypress Developer Community currently doesn’t allow sign-in to prepare for the upcoming transition. To learn more, check out our announcement.
cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Interfacing CYRF7936 with PSoC or any other Processor

Anonymous
Not applicable

Interfacing CYRF7936 with PSoC or any other Processor

Question: Can you interface CYRF7936 with PSoC or any processor and use it interface with USB port on PC ?

 

Answer:

The CYRF7936 is a transceiver (Tx and Rx). The CYRF7936 is a standalone radio with a SPI interface that can be connected to any processor with SPI and then the processor would interface to USB on the PC. Cypress recommends to use a PSoC for your microprocessor because the protocol is designed for the PSoC and the CYRF7936. PSOC will interface to the RF chip via SPI and also have USB connectivity to the Host (if CY8C24x94 device is used).

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Feb 09, 2009 12:00 AM
Updated by:
Anonymous
 
Contributors