cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

How to use USB Type-C/PD Controllers of HX3C in USB PD Compliant Hub - KBA212027

Anonymous
Not applicable

How to use USB Type-C/PD Controllers of HX3C in USB PD Compliant Hub - KBA212027

Version: **

Translation - Japanese: USB PD準拠ハブでHX3CのUSB Type-C/PDコントローラを使用する方法について- KBA212027- Community Translated (JA)

Question:

How to use USB Type-C/PD Controllers of HX3C in USB PD compliant hub?

Answer:

HX3C is a USB PD compliant hub with two integrated USB PD controllers. This allows to design a hub with two USB PD compliant Type-C ports, one in Upstream and one in Downstream.

One of the USB PD controllers is used for providing USB PD capability to the upstream port of HX3C, whereas the second USB PD controller can be used to add USB PD capability to any one of the available downstream ports DS1, DS2 or DS4.

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Apr 04, 2016 01:18 AM
Updated by:
Anonymous
 
Contributors