cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Global Out Net routing restrictions

DineshbabuM_66
Employee

Global Out Net routing restrictions

Question: Can I route different signals like two digital block outputs to same pins of two ports like P4[0] and P2[0]?

 

Answer:

Both P4[0] and P2[0] are connected to Global_Out_Even0 net.  As there cannot be two sources driving the same Global out net, it is not possible to route two different signals on these pins. For example, it is not possible to route a PWM output to P4[0] and UART TX output to P2[0].  Under such circumstances, select a different Global Output net for one of the signals and route it to a different pin.

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Feb 26, 2011 12:36 PM
Updated by:
 
Contributors