Fixing Compilation Errors While Updating UMs in PSoC® Designer™ 5.1, SP3 - KBA82259
Anonymous
Not applicable
Sep 27, 2012
05:40 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Sep 27, 2012
05:40 AM
Version: **
Question: How to fix the compilation errors due to EzI2C User Module been updated?
Answer:
In order to fix the compilation errors created due to EzI2C User Module (UM) update, simply delete the UM and replace it. This also effects the following UMs: CSD (StdUM), CSDADC and SmartSense when they are used with EzI2C.
There was an issue with UM update in PSoC Designer 5.1 Service Pack 3. During the UM update, new UM version set default parameters first (default pins), but later the parameters are restored from the old UM version. Therefore when update was finished, pin settings for the pins, intended to be default for CSD ("Feedback Resistor Pin" and "Modulator Capacitor Pin") were corrupted.
This issue is fixed and handled in the next service packs including SP4, SP5, and SP6 of PSoC Designer 5.1.
Labels
- Tags:
- psoc designer
Rate this article:
Contributors
-
This widget could not be displayed.Anonymous