Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

FX2LP Get Pipes Information Problems with Windows XP

FX2LP Get Pipes Information Problems with Windows XP

Anonymous
Not applicable
Question: Why does the Get Pipes information of Cyconsole not display when using the bulk transfer example using Windows XP?

 

Answer:

You should not experience any differences when using Windows 2000 or Windows XP with our bulk transfer examples. This problem can be caused by downloading an EZ-USB example instead of an FX2LP example or by not having the correct target set in the EZ-USB CyConsole control panel.

Ensure that the target in EZ-USB CyConsole control panel shows FX2LP and that the bulk transfer example Bulkloop downloaded is from the C:\Cypress\USB\Examples\FX2LP directory if you have installed the
CY3684 EZ-USB FX2LP Development Kit http://www.cypress.com/?rID=14321.
 

0 Likes
280 Views
Contributors