cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

FX2LPデバイスのシリアル番号を生成 – KBA212789 - Community Translated (JA)

SivaK_96
Employee

FX2LPデバイスのシリアル番号を生成 – KBA212789 - Community Translated (JA)

Community Translated by  NoTa_4591161    Version: *A

Translation - English: Generate Serial Number for a FX2LP Device – KBA212789

質問:

FX2LPデバイスのシリアル番号を生成するにはどうすればよいでしょうか?

回答:

シリアル番号は、デバイスを識別するために使用されます。これを使用すると、すべてのデバイスに固有の番号が付けられ、FX2LPパーツを簡単に区別できます。これは2つの方法で生成できます。

1.記述子ファイル(dscr.a51ファイル)にシリアル番号文字列を追加します。

SerialNum

      db SerialNum-SerialNumend   ;; ディスクリプタの長さ

      db DSCR_STRING

      db 00.00

      db 00.00

      db 00.00

      db 00.00

      db 00.00

      db 00.00

      db 00.00

      db 00.00

      db 00.00

      db 00.00

      db 00.00

      db 00.00

SerialNumEnd

最初の列には、選択した数を入力できます。この方法の欠点の1つは、すべてのデバイスのシリアル番号を手動で入力する必要があることです。

2.ファームウェアに関数を記述して、一意のシリアル番号を生成しますFX2LPには、各FX2LPデバイスに固有の6つのレジスタがあります。文字列ディスクリプタはこれらのレジスタの内容で更新され、接続されているすべてのFX2LPデバイスに一意のシリアル番号を生成します。実装については、添付のファームウェアプロジェクト(InsertSerialNumber()関数ブロック)をご参照願います。

Attachments
0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Jul 30, 2020 11:02 PM
Updated by:
 
Contributors