cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

External Master Reset of all Cypress FIFO's

Anonymous
Not applicable

External Master Reset of all Cypress FIFO's

Question: - Is there a built-in reset in Cypress FIFO's? - Is there POR circuitry in Cypress FIFO's? - Do I need to reset the FIFO on power up?

 

Answer:

All Cypress FIFO's require an external Master Reset cycle upon power up. There is no internal built-in circuitry for this. It is very important to complete a full Master Reset cycle, adhering to the specifications laid out in each device's datasheet. If a full Master Reset cycle is not issued upon start up, there is a high chance that the FIFO will not work properly. Please review the datasheet for the FIFO in question to find out the specific requirements for a Master Reset.

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Jun 13, 2011 11:06 AM
Updated by:
Anonymous
 
Contributors