Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

EZ-USB® FX3™ VBUS Power Consumption – KBA90951

EZ-USB® FX3™ VBUS Power Consumption – KBA90951

Anonymous
Not applicable
Version: **

 

Question: What is the FX3™ VBUS power consumption?

 

Answer:

Answer: Table 1 shows the FX3 VBUS power consumption for different power modes with VBatt disabled and enabled.

Table1. FX3 VBUS Power consumption in different modes

                                                         
    Power Mode    VBatt Disabled    VBatt Enabled
    Self Powered    20 mA (Bootloader)/
    23 mA (Application)
    20.0 uA ( Application)
    Bus Powered    148 mA (Bootloader)/
    233 mA (Application)
    NA
0 Likes
760 Views
Contributors