cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Current Rating of GPIO in encore V

saiprashanthc_
Employee

Current Rating of GPIO in encore V

Question: What the current ratings of GPIOs in CY7C6434x(encoreV)?

 

Answer:

The current ratings for encore V device are as follows:

Sink Current: 25 mA sink current on all GPIO
   60mA total sink current on Even Port pins and 60mA total sink current  on Odd Port pins
   120 mA total sink current on all GPIOs.

Source Current: CMOS drive mode – 5 mA source current on ports 0 and 1  and 1 mA on ports 2, 3, and 4
 20 mA total source current on all GPIOs.

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Sep 30, 2010 02:07 AM
Updated by:
 
Contributors