cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Configuring pipelined vs. flow-through mode after power up

Anonymous
Not applicable

Configuring pipelined vs. flow-through mode after power up

Question: Can the Flowthrough/Pipeline mode be reconfigured after power-up for some Full flex dual port SRAM's?

 

Answer:

The Flowthrough/Pipeline mode can be reconfigured after power-up. To do it safely, no other valid operation should be done during the *FT/PIPE change. It is recommended that you first disable the chip, then change *FT/PIPE pin (from VCC to GND or vice versa), then wait a cycle before resuming normal read and write operations.

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Jun 11, 2011 12:03 AM
Updated by:
Anonymous
 
Contributors