cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Configuration of P1[0] and P1[1] when not used

Anonymous
Not applicable

Configuration of P1[0] and P1[1] when not used

Question: How should the P1[0] and P1[1] be configured in the project if they are used only for ISSP?

 

Answer:

Pin P1[0] & P1[1] can be used for ISSP programming / I2C Interface / GPIO. If these pins are not used except for ISSP programming, they may be left at their default state of StdCPU / HighZ Analog in the device editor.

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Mar 27, 2011 04:31 PM
Updated by:
Anonymous
 
Contributors